The maximum load is defined by the static basic load rating C0. If static loads are a combination of radial and axial loads, the equivalent static load will have to be calculated.
For Rod Ends with integral self-aligning ball bearing 65740, 65742, 65760, 65820, 65840.
Rotating
Oscillating
For Rod ends with integral self-aligning roller bearing 65780, 65800.
Rotating
Oscillating
At the rotating side of a crank mechanism a ball or roller bearing rod end should be installed. The expected service life amounts to at least 5000 hours.