Use hard metals such as stainless steels for the base panel.
Spacing tolerance on both the sub panel and the base panel should be ±0.1.
For highly accurate locating, use locating pins 36340 or 36341. Repeatability of ±0.25
is achievable.