Hydraulic and pneumatic components and systems are often cross-drilled to provide the correct channels for aid and gas. Some of these channels have to be drilled from the outside and later need to be closed off (plugged).
The Expansions Sealing Plugs are inserted into a drilled hole and the expander ball is driven into the plug sleeve. The independent grooved sealing rings on the plug ball are driven into the housing material to permanently plug and seal the hole. The ball is retained in place.
No need for tapping or reaming, no machining of O-ring grooves or the use of tapes or sealants. To seal a hole, follow this procedure:
Standard series expansion sealing plugs. Available in zinc plated steel, stainless steel (A2 or A4) and aluminium. Ideal for blanking off externally drilled holes for air and gas.
Stainless steel (A2) expansion retractors for restricting flow, with calibrated hole diameter. Available in imperial or metric with orders to specific sizes.
Pan head. Integral Sealing Screws feature an O-ring underneath the screw, to provide bi-direction sealing. This makes them ideal for protection against contaminates such as a dirt.
Blanking Plug Sealing Screw for creating bi-directional seals. Ideal for use in applications where foreign contaminates such as dirt are an issue.
Some of the typical applications for our Sealing Screws include:
"Standard" Expansion Sealing Plugs - push the ball which expands the sleeve and seals the channel.
"Pull" Expansion Sealing Plugs. Pulling on the mandrel expands the sleeve, sealing the channel. At a predetermined force, the mandrel breaks off.
There is a direct connection between the necessary drilling roughnesses required and both the hardness and the tensile characteristics of the base material. Depending on the mounting combination of Sealing Plug and base material, anchorage can either take place via the rifle profile of the expansion sleeve (automatic anchorage) or via the surface of the drilling hole.
Depending on the type of Expansion Sealing Plug and the hardness of the base material, a bore roughness of Rz= 10 - 30µm has to be adhered to. Requirements to achieve maximum operation reliability:
In cases, where an automatic anchorage is not possible when building in the Expander Sealing Plug into a hard base material a drilling roughness of:
Automatic Anchorage
Example: Expansion Sealing Plug made from case hardened steel HB = 180, in aluminium alloy HB = 90.
Required roughness design - An ideal bore roughness for the anchor can be achieved by using a twist drill or countersink.
Undesirable roughness design - Friction will cause a smooth roughness profile that is not desired.