The maximum load is defined by the static basic load rating C0. If static loads are a combination of radial and axial loads, the equivalent static load will have to be calculated.
For Rod Ends with integral self-aligning Ball Bearing 65740, 65742, 65760, 65820, 65840.
Rotating
Oscillating
For Rod Ends with integral self-aligning Roller Bearing 65780, 65800.
Rotating
Oscillating
At the rotating side of a crank mechanism, a Ball or Roller Bearing Rod End should be installed. The expected service life amounts to at least 5000 hours.