Our Horizontal Clamps have a unique "three finger" arrangement, ensuring components are both pulled down and clamped in the same motion. The face of the clamp is made of three parts or fingers:
Available in two styles: smooth and serrated face. They can also cater for workpieces with an adverse angle on the clamping face for example, flame cuts steel blanks.
Quick 1/4 turn eccentric clamping - on models offering 4000 and 12000 Newtons clamping force.
Rear screw clamping - on models offering 6500, 10000 and 22000 Newtons clamping force.
T-Slotted tables
Dedicated fixturing
Modular Fixturing.
Yes, the 12031 Pitbull Clamps exert down force as well as a sideway holding force.
The oil resistant o-ring has two main purposes, the first is two prevent oil from getting into the thread which could loosen the clamp, the second purpose is act as a spring when unclamping.
Yes, we sell a Mitee-bite vice jaw set which is a simple bolt mounted system. Once you have bolted on the vice jaws to your vice, you then use the talon grip clamps which come with the set to clamp the component. Clamping can be on as little as 1,5mm.
Yes, the Mitee-bite t-slot fixture clamps 12150 will be ideal to clamp components on a t-slot table. The clamp uses a cam action to provide fast and strong clamping.