Four ball bearings clamp onto the clamping pin, the wedge shape of the pin (33929) draws the panels together during clamping.
Rotation of either sub panel or base panel can result in one touch fastener unclamping. When either panel is at risk of rotating, ensure a stop is in place.
For highly accurate locating, use locating components 36340 or 36341. Repeatability of ±0.25 is achievable.
Spacing tolerance on both the sub plate and the base plate should be ±0.1.