You can slide the steel bar when the knob is at the "OFF" position since there is clearance between the steel bar and the shafts.
The steel bar is locked when the knob is at the "ON" position since the shafts are pushed by the wedge.
Please refer to notes for safe use (last page of guide).
Usable Materials: Flat bar (JIS h14 grade) made of SS400,
S45C or SUS304 etc.
Machining of slotted hole: Recommended tolerance of the slotted hole to prevent chattering is shown left.
For more accurate sliding, machine the slotted hole to fit the dimension of 10mm (-0.05 to 0) on the bottom of sliding locks. Remove the burr around the slotted hole to ensure locking.
Can be used for various steel thicknesses by attaching the riser plates (ordered separately, see 33971).
You can read the scale with the line on the body of the sliding lock.
Scale plate is separately available.
See ranges 33975, 33976 and 33977.
The displacement of steel bar by axial load (static load from single direction)
Note: The data is for a flat bar made of SUS304 stainless steel, SS400 steel and S45C steel. Using an aluminium flat bar the surface will be scratched or dent by applied load.