You can slide the steel bar when the knob is at the “OFF” position since there is clearance between the steel bar and the shafts.
The steel bar is locked when the knob is at the “ON” position since the shafts are pushed by the wedge.
The steel bar can slide to right and left at the “OFF” position. The steel bar is locked at the “ON” position.
Note: The knob clicks at the “ON” and “OFF” positions, and this enables the operators to lock/unlock securely.
Please refer to notes for safe use (see last page of guide).
Usable Materials: Flat bar (JIS h14 grade) made of SS400, S45C or SUS304 etc.
Riser plates (to be ordered separately) can lift the steel bar to create a clearance between the steel bar and the base.
Can be used with attachments such as pointer plates and brackets.
Scale plate can be put on the steel bar.
Note: Fit scale plate inside the slot in the figure below. Putting scale plate outside the slot cause interference between scale plate and sliding lock.
Scale plate is separately available.
See ranges 33975, 33976 and 33977.
A: For bar width x heights; 12x12mm and 16x16mm.
B: For bar width x heights; 25x9, 25x12, 32x12, 32x16.
Note: This data is for a flat bar base of SUS304 stainless steel, SS400 steel and S45C steel. Using an aluminum flat bar, the surface will be scratched or dented by applied load.