The Internal Centering Clamp provides autocentric chucking inside both round and square holes, at the simple turn of a hexagon screw. Precise self-centering is achieved through the expansion of the ring of balls which, during clamping, are pressed outward across a precision cone. As the outer diameter of the clamp changes, the balls transmit force between its body and the bore. The Clamps are used in machining and welding fixtures, product assemblies and transfer units.
Be the first to receive the latest news and exclusive offers via our newsletter.
Company registration no: 00496138
Company VAT number GB 408154022
Alexia House, Glenmore Business Park
PO19 7BJ Chichester
United Kingdom
0333 207 4497
sales@wixroyd.com